StackHorizontalAlignment Enumeration

class NXOpen.Annotations.StackHorizontalAlignment

Bases: object

Specifies the horizontal alignment(left/right alignment) option when aligning annotations within a stack Enum Members

Enum Member Enum Member Description
Top Align horizontally along top edge of text box
Middle Align horizontally along middle line of text box
Bottom Align horizontally along bottom edge of text box
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.