SizeLetterCode Enumeration

class NXOpen.Annotations.SizeLetterCode

Bases: object

Specifies the weld size letter code (ISO and DIN only) Enum Members

ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.