SingleSidedDisplayBuilder Class¶
-
class
NXOpen.Annotations.
SingleSidedDisplayBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Annotations.SingleSidedDisplayBuilder
.This is a sub-builder class and cannot be directly instantiated
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
DisplayAsSingleSided | Returns or sets the display as single sided |
SingleSidedArrowLineLength | Returns or sets the arrow line length on the open side of single sided dimension |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Flip | Flips the side of single sided dimension |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DisplayAsSingleSided¶
-
SingleSidedDisplayBuilder.
DisplayAsSingleSided
¶ Returns or sets the display as single sided
-------------------------------------
Getter Method
Signature
DisplayAsSingleSided
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplayAsSingleSided
Parameters: displayAsSingleSided (bool) – New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
SingleSidedArrowLineLength¶
-
SingleSidedDisplayBuilder.
SingleSidedArrowLineLength
¶ Returns or sets the arrow line length on the open side of single sided dimension
-------------------------------------
Getter Method
Signature
SingleSidedArrowLineLength
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SingleSidedArrowLineLength
Parameters: singleSidedArrowLineLength (float) – New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Flip¶
-
SingleSidedDisplayBuilder.
Flip
¶ Flips the side of single sided dimension
Signature
Flip()
New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
Validate¶
-
SingleSidedDisplayBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.