ShipDraftingFramebarGeneralBuilderTicDirectionTypes Enumeration

NXOpen.Annotations.ShipDraftingFramebarGeneralBuilder.TicDirectionTypes is an alias for NXOpen.Annotations.ShipDraftingFramebarGeneralBuilderTicDirectionTypes

class NXOpen.Annotations.ShipDraftingFramebarGeneralBuilderTicDirectionTypes

Bases: object

Tic Direction Options

Enum Members

Enum Member Enum Member Description
TowardsView
AwayfromView
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.