SearchModelViewBuilderValueComparisionOptions Enumeration

NXOpen.Annotations.SearchModelViewBuilder.ValueComparisionOptions is an alias for NXOpen.Annotations.SearchModelViewBuilderValueComparisionOptions

class NXOpen.Annotations.SearchModelViewBuilderValueComparisionOptions

Bases: object

Represents the value comparision options

Enum Members

Enum Member Enum Member Description
Less
LessEqual
Equal
MoreEqual
More
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.