SearchCriteriaSurfaceFinishBuilderToleranceTypeOptions Enumeration¶
NXOpen.Annotations.SearchCriteriaSurfaceFinishBuilder.ToleranceTypeOptions is an alias for NXOpen.Annotations.SearchCriteriaSurfaceFinishBuilderToleranceTypeOptions
-
class
NXOpen.Annotations.
SearchCriteriaSurfaceFinishBuilderToleranceTypeOptions
¶ Bases:
object
Lists the Tolerance type of surface finish value
Enum Members
Enum Member Enum Member Description NoTolerance no tolerance EqualBilateral equal bilateral Bilateral bilateral UnilateralPlus unilateral + UnilateralMinus unilateral - PlusLimit2Lines - limit 2 lines
MinusLimit2Lines - limit 2 lines
PlusLimit1Line - limit 1 line
NegposlimitMinusLimit1Line negposlimit- limit 1 line -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.