SearchCriteriaFeatureControlFrameBuilderIndicatorOptions Enumeration¶
NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilder.IndicatorOptions is an alias for NXOpen.Annotations.SearchCriteriaFeatureControlFrameBuilderIndicatorOptions
-
class
NXOpen.Annotations.
SearchCriteriaFeatureControlFrameBuilderIndicatorOptions
¶ Bases:
object
Lists the status of pmi feature control frame indicator
Enum Members
Enum Member Enum Member Description Yes have indicator No have no indicator -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-