SearchCriteriaDimensionBuilderDimensionTypes Enumeration¶
NXOpen.Annotations.SearchCriteriaDimensionBuilder.DimensionTypes is an alias for NXOpen.Annotations.SearchCriteriaDimensionBuilderDimensionTypes
-
class
NXOpen.Annotations.
SearchCriteriaDimensionBuilderDimensionTypes
¶ Bases:
object
Specifies dimension types
Enum Members
Enum Member Enum Member Description Linear Linear Angular Angular Diameter Diameter Radial Radial Chamfer Chamfer Thickness Thickness ArcLength ArcLength Chain Chain Ordinate Ordinate Baseline Baseline -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-