RadialStyleBuilder Class¶
-
class
NXOpen.Annotations.
RadialStyleBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Annotations.RadialStyleBuilder
.This class queries and sets preferences specific to radial dimensions when creating or editing a radial type dimension.
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
DiameterRadiusPlacement | Returns or sets the diameter radius symbol placement with respect to the dimension text. |
DiameterSymbol | Returns or sets the text for a user-defined diameter symbol |
DiameterSymbolType | Returns or sets the diameter symbol type |
FoldedRadiusAngle | Returns or sets the folded radius angle |
RadiusSymbol | Returns or sets the text for a user-defined radius symbol |
RadiusSymbolType | Returns or sets the radius symbol type |
SymbolToDimensionTextDistance | Returns or sets the symbol to dimension text distance in character spaces |
Tag | Returns the Tag for this object. |
TextAboveLeader | Returns or sets the location of the dimension text relative to the leader stub |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DiameterRadiusPlacement¶
-
RadialStyleBuilder.
DiameterRadiusPlacement
¶ Returns or sets the diameter radius symbol placement with respect to the dimension text.
One of the options specifies that no symbol be displayed
-------------------------------------
Getter Method
Signature
DiameterRadiusPlacement
Returns: Return type: NXOpen.Annotations.DiameterRadiusSymbolPlacement
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DiameterRadiusPlacement
Parameters: diameterRadiusPlacement ( NXOpen.Annotations.DiameterRadiusSymbolPlacement
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
DiameterSymbol¶
-
RadialStyleBuilder.
DiameterSymbol
¶ Returns or sets the text for a user-defined diameter symbol
-------------------------------------
Getter Method
Signature
DiameterSymbol
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DiameterSymbol
Parameters: diameterSymbol (str) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
DiameterSymbolType¶
-
RadialStyleBuilder.
DiameterSymbolType
¶ Returns or sets the diameter symbol type
-------------------------------------
Getter Method
Signature
DiameterSymbolType
Returns: Return type: NXOpen.Annotations.DiameterSymbol
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DiameterSymbolType
Parameters: diameterSymbolType ( NXOpen.Annotations.DiameterSymbol
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FoldedRadiusAngle¶
-
RadialStyleBuilder.
FoldedRadiusAngle
¶ Returns or sets the folded radius angle
-------------------------------------
Getter Method
Signature
FoldedRadiusAngle
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FoldedRadiusAngle
Parameters: foldedRadiusAngle (float) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
RadiusSymbol¶
-
RadialStyleBuilder.
RadiusSymbol
¶ Returns or sets the text for a user-defined radius symbol
-------------------------------------
Getter Method
Signature
RadiusSymbol
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RadiusSymbol
Parameters: radiusSymbol (str) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
RadiusSymbolType¶
-
RadialStyleBuilder.
RadiusSymbolType
¶ Returns or sets the radius symbol type
-------------------------------------
Getter Method
Signature
RadiusSymbolType
Returns: Return type: NXOpen.Annotations.RadiusSymbol
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RadiusSymbolType
Parameters: radiusSymbolType ( NXOpen.Annotations.RadiusSymbol
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SymbolToDimensionTextDistance¶
-
RadialStyleBuilder.
SymbolToDimensionTextDistance
¶ Returns or sets the symbol to dimension text distance in character spaces
-------------------------------------
Getter Method
Signature
SymbolToDimensionTextDistance
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SymbolToDimensionTextDistance
Parameters: symbolToDimensionTextDistance (float) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
TextAboveLeader¶
-
RadialStyleBuilder.
TextAboveLeader
¶ Returns or sets the location of the dimension text relative to the leader stub
-------------------------------------
Getter Method
Signature
TextAboveLeader
Returns: Return type: NXOpen.Annotations.DiameterRadiusLeaderStub
New in version NX6.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.Annotations.DimensionStyleBuilder.TextPosition()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
TextAboveLeader
Parameters: textAboveLeader ( NXOpen.Annotations.DiameterRadiusLeaderStub
) –New in version NX6.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.Annotations.DimensionStyleBuilder.TextPosition()
instead.License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
RadialStyleBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.