PmiFilterByTypeType Enumeration¶
NXOpen.Annotations.PmiFilterByType.Type is an alias for NXOpen.Annotations.PmiFilterByTypeType
-
class
NXOpen.Annotations.
PmiFilterByTypeType
¶ Bases:
object
Represents a PMI type that is assigned to the PMI filter.
Enum Members
Enum Member Enum Member Description Dimension Indicates a PMI dimension type FeatureControlFrame Indicates a PMI feature control frame type Datum Indicates a PMI datum feature type DatumTarget Indicates a PMI datum target type Note Indicates a PMI note type GeneralNote Indicates a PMI general note type SpecificNote Indicates a PMI specific note type CoordinateNote Indicates a PMI coordinate note type BalloonNote Indicates a PMI balloon type CustomSymbol Indicates a PMI custom symbol type Centerline Indicates a PMI centerline type LineWeld Indicates a PMI weld type Crosshatch Indicates a PMI crosshatch type Material Indicates a PMI material type SurfaceFinish Indicates a PMI surface finish type Locator Indicates a PMI locator type EnterpriseIdentifier Indicates a PMI enterprise identifier type Process Indicates a PMI process type PartIdentifier Indicates a PMI part identifier type Emarking Indicates a PMI e-Marking type Url Indicates a PMI URL type UserDefined Indicates a PMI user defined type Geometry Indicates a PMI Geometry type CuttingPlaneSymbol Indicates a PMI Cutting Symbol Type Table Indicates a PMI Table Type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-