PmiBoltCircleCenterlineBuilder Class¶
-
class
NXOpen.Annotations.
PmiBoltCircleCenterlineBuilder
¶ Bases:
NXOpen.Annotations.BaseBoltCircleCenterlineBuilder
Builder for creating or editing PMI Bolt Circle Centerline
To create a new instance of this class, use
NXOpen.Annotations.CenterlineCollection.CreatePmiBoltCircleCenterlineBuilder()
Default values.
Property Value FullCircle true Type Through3Points New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
AssociatedObjects | Returns the associated objects for the center mark |
FullCircle | Returns or sets the method which returns full or partial circle flag |
Inherit | Returns the inherit object |
Locations | Returns the selction object of the centerline |
Plane | Returns the plane for the creation of center mark |
Settings | Returns the settings builder object for the centerline |
Tag | Returns the Tag for this object. |
Type | Returns or sets the method which returns type of centerline |
Methods¶
Method | Description |
---|---|
AddEndExtensions | Adds extensions only at ends |
AddExtension | Adds extension based on select object index |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAllExtensions | Returns all extensions. |
GetAllIndividualExtensions | Returns individual extensions. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetEndExtensions | Returns end extensions only. |
GetObject | Returns the object currently being edited by this builder. |
RemoveEndExtensions | Removes extensions only at ends |
RemoveExtension | Removes extension based on select object index |
RemoveLocation | Removes location object for a given index from the Select Object List. |
ResetAllExtensions | Reset all extensions by the supplied defaultValue |
SetAllIndividualExtensions | Sets all individual extensions |
SetEndExtensions | Modifies end extensions only |
SetIndividualExtensions | Modifies extensions based on select object index |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AssociatedObjects¶
-
PmiBoltCircleCenterlineBuilder.
AssociatedObjects
¶ Returns the associated objects for the center mark
-------------------------------------
Getter Method
Signature
AssociatedObjects
Returns: Return type: NXOpen.Annotations.AssociatedObjectsBuilder
New in version NX12.0.0.
License requirements: None.
Plane¶
-
PmiBoltCircleCenterlineBuilder.
Plane
¶ Returns the plane for the creation of center mark
-------------------------------------
Getter Method
Signature
Plane
Returns: Return type: NXOpen.Annotations.PlaneBuilder
New in version NX12.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
PmiBoltCircleCenterlineBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.