PmiAttributeCollection Class

class NXOpen.Annotations.PmiAttributeCollection

Bases: object

Represents a collection of NXOpen.Annotations.PmiAttribute objects.

To obtain an instance of this class, refer to NXOpen.Annotations.PmiManager

New in version NX6.0.0.

Methods

Method Description
CreateBalloonNoteBuilder Creates a NXOpen.Annotations.BalloonNoteBuilder
CreateCompanyProprietaryInformationBuilder Creates a NXOpen.Annotations.CompanyProprietaryInformationBuilder
CreateCoordinateNoteBuilder Creates a NXOpen.Annotations.CoordinateNoteBuilder
CreateEnterpriseIdentificationBuilder Creates a NXOpen.Annotations.EnterpriseIdentificationBuilder
CreateExportControlBuilder Creates a NXOpen.Annotations.ExportControlBuilder
CreateGeneralNoteBuilder Creates a NXOpen.Annotations.GeneralNoteBuilder
CreateGovernmentSecurityInformationBuilder Creates a NXOpen.Annotations.GovernmentSecurityInformationBuilder
CreateLocatorDesignatorBuilder Creates a NXOpen.Annotations.LocatorDesignatorBuilder
CreateMaterialSpecificationBuilder Creates a NXOpen.Annotations.MaterialSpecificationBuilder
CreatePartIdentificationBuilder Creates a NXOpen.Annotations.PartIdentificationBuilder
CreatePmiAttributeBuilder Creates a NXOpen.Annotations.PmiAttributeBuilder
CreatePmiAttributeValueIntegerBuilder Creates a NXOpen.Annotations.PmiAttributeValueIntegerBuilder
CreatePmiAttributeValueListBuilder Creates a NXOpen.Annotations.PmiAttributeValueListBuilder
CreatePmiAttributeValueMultipleStringBuilder Creates a NXOpen.Annotations.PmiAttributeValueMultipleStringBuilder
CreatePmiAttributeValueNumberBuilder Creates a NXOpen.Annotations.PmiAttributeValueNumberBuilder
CreatePmiAttributeValueStringBuilder Creates a NXOpen.Annotations.PmiAttributeValueStringBuilder
CreatePmiAttributeValueUrlBuilder Creates a NXOpen.Annotations.PmiAttributeValueUrlBuilder
CreatePmiIntegerBuilder Creates a NXOpen.Annotations.PmiIntegerBuilder
CreatePmiNumberBuilder Creates a NXOpen.Annotations.PmiNumberBuilder
CreatePmiStringBuilder Creates a NXOpen.Annotations.PmiStringBuilder
CreatePmiUrlNoteBuilder Creates a NXOpen.Annotations.PmiUrlNoteBuilder
CreatePmiUserDefinedBuilder Creates a NXOpen.Annotations.PmiUserDefinedBuilder
CreateProcessSpecificationBuilder Creates a NXOpen.Annotations.ProcessSpecificationBuilder
CreateSpecificNoteBuilder Creates a NXOpen.Annotations.SpecificNoteBuilder
CreateSurfaceFinishBuilder Creates a NXOpen.Annotations.SurfaceFinishBuilder
FindObject Finds the NXOpen.Annotations.PmiAttribute with the given identifier as recorded in a journal.

Method Detail

CreateBalloonNoteBuilder

PmiAttributeCollection.CreateBalloonNoteBuilder

Creates a NXOpen.Annotations.BalloonNoteBuilder

Signature CreateBalloonNoteBuilder(balloonNote)

Parameters:balloonNote (NXOpen.Annotations.BalloonNote) – balloon note
Returns:
Return type:NXOpen.Annotations.BalloonNoteBuilder

New in version NX6.0.0.

License requirements: None.

CreateCompanyProprietaryInformationBuilder

PmiAttributeCollection.CreateCompanyProprietaryInformationBuilder

Creates a NXOpen.Annotations.CompanyProprietaryInformationBuilder

Signature CreateCompanyProprietaryInformationBuilder(companyProprietaryInformation)

Parameters:companyProprietaryInformation (NXOpen.Annotations.CompanyProprietaryInformation) – company proprietary
Returns:
Return type:NXOpen.Annotations.CompanyProprietaryInformationBuilder

New in version NX6.0.0.

License requirements: None.

CreateCoordinateNoteBuilder

PmiAttributeCollection.CreateCoordinateNoteBuilder

Creates a NXOpen.Annotations.CoordinateNoteBuilder

Signature CreateCoordinateNoteBuilder(coordinateNote)

Parameters:coordinateNote (NXOpen.Annotations.CoordinateNote) – coordinate note
Returns:
Return type:NXOpen.Annotations.CoordinateNoteBuilder

New in version NX6.0.0.

License requirements: None.

CreateEnterpriseIdentificationBuilder

PmiAttributeCollection.CreateEnterpriseIdentificationBuilder

Creates a NXOpen.Annotations.EnterpriseIdentificationBuilder

Signature CreateEnterpriseIdentificationBuilder(enterpriseIdentification)

Parameters:enterpriseIdentification (NXOpen.Annotations.EnterpriseIdentification) – enterprise identification
Returns:
Return type:NXOpen.Annotations.EnterpriseIdentificationBuilder

New in version NX6.0.0.

License requirements: None.

CreateExportControlBuilder

PmiAttributeCollection.CreateExportControlBuilder

Creates a NXOpen.Annotations.ExportControlBuilder

Signature CreateExportControlBuilder(exportControl)

Parameters:exportControl (NXOpen.Annotations.ExportControl) – export control
Returns:
Return type:NXOpen.Annotations.ExportControlBuilder

New in version NX6.0.0.

License requirements: None.

CreateGeneralNoteBuilder

PmiAttributeCollection.CreateGeneralNoteBuilder

Creates a NXOpen.Annotations.GeneralNoteBuilder

Signature CreateGeneralNoteBuilder(generalNote)

Parameters:generalNote (NXOpen.Annotations.GeneralNote) – general note
Returns:
Return type:NXOpen.Annotations.GeneralNoteBuilder

New in version NX6.0.0.

License requirements: None.

CreateGovernmentSecurityInformationBuilder

PmiAttributeCollection.CreateGovernmentSecurityInformationBuilder

Creates a NXOpen.Annotations.GovernmentSecurityInformationBuilder

Signature CreateGovernmentSecurityInformationBuilder(governmentSecurityInformation)

Parameters:governmentSecurityInformation (NXOpen.Annotations.GovernmentSecurityInformation) – eMarking government
Returns:
Return type:NXOpen.Annotations.GovernmentSecurityInformationBuilder

New in version NX6.0.0.

License requirements: None.

CreateLocatorDesignatorBuilder

PmiAttributeCollection.CreateLocatorDesignatorBuilder

Creates a NXOpen.Annotations.LocatorDesignatorBuilder

Signature CreateLocatorDesignatorBuilder(locatorDesignator)

Parameters:locatorDesignator (NXOpen.Annotations.LocatorDesignator) – locator designator
Returns:
Return type:NXOpen.Annotations.LocatorDesignatorBuilder

New in version NX6.0.0.

License requirements: None.

CreateMaterialSpecificationBuilder

PmiAttributeCollection.CreateMaterialSpecificationBuilder

Creates a NXOpen.Annotations.MaterialSpecificationBuilder

Signature CreateMaterialSpecificationBuilder(materialSpecification)

Parameters:materialSpecification (NXOpen.Annotations.MaterialSpecification) – material specification
Returns:
Return type:NXOpen.Annotations.MaterialSpecificationBuilder

New in version NX6.0.0.

License requirements: None.

CreatePartIdentificationBuilder

PmiAttributeCollection.CreatePartIdentificationBuilder

Creates a NXOpen.Annotations.PartIdentificationBuilder

Signature CreatePartIdentificationBuilder(partIdentification)

Parameters:partIdentification (NXOpen.Annotations.PartIdentification) – part identification
Returns:
Return type:NXOpen.Annotations.PartIdentificationBuilder

New in version NX6.0.0.

License requirements: None.

CreatePmiAttributeBuilder

PmiAttributeCollection.CreatePmiAttributeBuilder

Creates a NXOpen.Annotations.PmiAttributeBuilder

Signature CreatePmiAttributeBuilder(pmiAttr)

Parameters:pmiAttr (NXOpen.Annotations.PmiAttribute) – pmi base class
Returns:
Return type:NXOpen.Annotations.PmiAttributeBuilder

New in version NX6.0.0.

License requirements: None.

CreatePmiAttributeValueIntegerBuilder

PmiAttributeCollection.CreatePmiAttributeValueIntegerBuilder

Creates a NXOpen.Annotations.PmiAttributeValueIntegerBuilder

Signature CreatePmiAttributeValueIntegerBuilder(pmiAttributeValueInteger)

Parameters:pmiAttributeValueInteger (NXOpen.Annotations.PmiAttributeValueInteger) – integer value
Returns:
Return type:NXOpen.Annotations.PmiAttributeValueIntegerBuilder

New in version NX6.0.0.

License requirements: None.

CreatePmiAttributeValueListBuilder

PmiAttributeCollection.CreatePmiAttributeValueListBuilder

Creates a NXOpen.Annotations.PmiAttributeValueListBuilder

Signature CreatePmiAttributeValueListBuilder(pmiAttributeValueList)

Parameters:pmiAttributeValueList (NXOpen.Annotations.PmiAttributeValueList) – list value
Returns:
Return type:NXOpen.Annotations.PmiAttributeValueListBuilder

New in version NX6.0.0.

License requirements: None.

CreatePmiAttributeValueMultipleStringBuilder

PmiAttributeCollection.CreatePmiAttributeValueMultipleStringBuilder

Creates a NXOpen.Annotations.PmiAttributeValueMultipleStringBuilder

Signature CreatePmiAttributeValueMultipleStringBuilder(pmiAttributeValueMultipleString)

Parameters:pmiAttributeValueMultipleString (NXOpen.Annotations.PmiAttributeValueMultipleString) – multiple string value
Returns:
Return type:NXOpen.Annotations.PmiAttributeValueMultipleStringBuilder

New in version NX6.0.0.

License requirements: None.

CreatePmiAttributeValueNumberBuilder

PmiAttributeCollection.CreatePmiAttributeValueNumberBuilder

Creates a NXOpen.Annotations.PmiAttributeValueNumberBuilder

Signature CreatePmiAttributeValueNumberBuilder(pmiAttributeValueNumber)

Parameters:pmiAttributeValueNumber (NXOpen.Annotations.PmiAttributeValueNumber) – number value
Returns:
Return type:NXOpen.Annotations.PmiAttributeValueNumberBuilder

New in version NX6.0.0.

License requirements: None.

CreatePmiAttributeValueStringBuilder

PmiAttributeCollection.CreatePmiAttributeValueStringBuilder

Creates a NXOpen.Annotations.PmiAttributeValueStringBuilder

Signature CreatePmiAttributeValueStringBuilder(pmiAttributeValueString)

Parameters:pmiAttributeValueString (NXOpen.Annotations.PmiAttributeValueString) – string value
Returns:
Return type:NXOpen.Annotations.PmiAttributeValueStringBuilder

New in version NX6.0.0.

License requirements: None.

CreatePmiAttributeValueUrlBuilder

PmiAttributeCollection.CreatePmiAttributeValueUrlBuilder

Creates a NXOpen.Annotations.PmiAttributeValueUrlBuilder

Signature CreatePmiAttributeValueUrlBuilder(pmiAttributeValueUrl)

Parameters:pmiAttributeValueUrl (NXOpen.Annotations.PmiAttributeValueUrl) – list value
Returns:
Return type:NXOpen.Annotations.PmiAttributeValueUrlBuilder

New in version NX6.0.0.

License requirements: None.

CreatePmiIntegerBuilder

PmiAttributeCollection.CreatePmiIntegerBuilder

Creates a NXOpen.Annotations.PmiIntegerBuilder

Signature CreatePmiIntegerBuilder(pmiInteger)

Parameters:pmiInteger (NXOpen.Annotations.PmiInteger) – integer
Returns:
Return type:NXOpen.Annotations.PmiIntegerBuilder

New in version NX6.0.0.

License requirements: None.

CreatePmiNumberBuilder

PmiAttributeCollection.CreatePmiNumberBuilder

Creates a NXOpen.Annotations.PmiNumberBuilder

Signature CreatePmiNumberBuilder(pmiNumber)

Parameters:pmiNumber (NXOpen.Annotations.PmiNumber) – number
Returns:
Return type:NXOpen.Annotations.PmiNumberBuilder

New in version NX6.0.0.

License requirements: None.

CreatePmiStringBuilder

PmiAttributeCollection.CreatePmiStringBuilder

Creates a NXOpen.Annotations.PmiStringBuilder

Signature CreatePmiStringBuilder(pmiString)

Parameters:pmiString (NXOpen.Annotations.PmiString) – string
Returns:
Return type:NXOpen.Annotations.PmiStringBuilder

New in version NX6.0.0.

License requirements: None.

CreatePmiUrlNoteBuilder

PmiAttributeCollection.CreatePmiUrlNoteBuilder

Creates a NXOpen.Annotations.PmiUrlNoteBuilder

Signature CreatePmiUrlNoteBuilder(pmiUrlNote)

Parameters:pmiUrlNote (NXOpen.Annotations.PmiUrlNote) – url note
Returns:
Return type:NXOpen.Annotations.PmiUrlNoteBuilder

New in version NX6.0.0.

License requirements: None.

CreatePmiUserDefinedBuilder

PmiAttributeCollection.CreatePmiUserDefinedBuilder

Creates a NXOpen.Annotations.PmiUserDefinedBuilder

Signature CreatePmiUserDefinedBuilder(userDefined)

Parameters:userDefined (NXOpen.Annotations.PmiUserDefined) – user defined
Returns:
Return type:NXOpen.Annotations.PmiUserDefinedBuilder

New in version NX6.0.0.

License requirements: None.

CreateProcessSpecificationBuilder

PmiAttributeCollection.CreateProcessSpecificationBuilder

Creates a NXOpen.Annotations.ProcessSpecificationBuilder

Signature CreateProcessSpecificationBuilder(processSpecification)

Parameters:processSpecification (NXOpen.Annotations.ProcessSpecification) – process specification
Returns:
Return type:NXOpen.Annotations.ProcessSpecificationBuilder

New in version NX6.0.0.

License requirements: None.

CreateSpecificNoteBuilder

PmiAttributeCollection.CreateSpecificNoteBuilder

Creates a NXOpen.Annotations.SpecificNoteBuilder

Signature CreateSpecificNoteBuilder(specificNote)

Parameters:specificNote (NXOpen.Annotations.SpecificNote) – specific note
Returns:
Return type:NXOpen.Annotations.SpecificNoteBuilder

New in version NX6.0.0.

License requirements: None.

CreateSurfaceFinishBuilder

PmiAttributeCollection.CreateSurfaceFinishBuilder

Creates a NXOpen.Annotations.SurfaceFinishBuilder

Signature CreateSurfaceFinishBuilder(surfaceFinish)

Parameters:surfaceFinish (NXOpen.Annotations.SurfaceFinish) – surface finish
Returns:
Return type:NXOpen.Annotations.SurfaceFinishBuilder

New in version NX6.0.0.

License requirements: None.

FindObject

PmiAttributeCollection.FindObject

Finds the NXOpen.Annotations.PmiAttribute with the given identifier as recorded in a journal.

An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.

An exception will be thrown if no object can be found with the given journal identifier.

Signature FindObject(journalIdentifier)

Parameters:journalIdentifier (str) – Identifier of the pmi
Returns:PMI with this identifier
Return type:NXOpen.TaggedObject

New in version NX6.0.0.

License requirements: None.