PlaneBuilderPlaneMethodType Enumeration¶
NXOpen.Annotations.PlaneBuilder.PlaneMethodType is an alias for NXOpen.Annotations.PlaneBuilderPlaneMethodType
-
class
NXOpen.Annotations.
PlaneBuilderPlaneMethodType
¶ Bases:
object
method used to compute the annotation plane
Enum Members
Enum Member Enum Member Description XyPlane XY of the WCS XzPlane XZ of the WCS YzPlane YZ of the WCS ModelView Model view plane UserDefined User define plane -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-