PinListBuilderFilterType Enumeration

NXOpen.Annotations.PinListBuilder.FilterType is an alias for NXOpen.Annotations.PinListBuilderFilterType

class NXOpen.Annotations.PinListBuilderFilterType

Bases: object

The options specify the filter type.

Enum Members

Enum Member Enum Member Description
RoutedandUnroutedConnections
OnlyRoutedConnections
OnlyUnroutedConnections
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.