PartsListBuilderPartsListSymbolType Enumeration¶
NXOpen.Annotations.PartsListBuilder.PartsListSymbolType is an alias for NXOpen.Annotations.PartsListBuilderPartsListSymbolType
-
class
NXOpen.Annotations.
PartsListBuilderPartsListSymbolType
¶ Bases:
object
Symbol Types The types specify the balloon type used to call out members
Enum Members
Enum Member Enum Member Description NotSet Circle DividedCircle TrianglePointedDown TrianglePointedUp Square DividedSquare Hexagon DividedHexagon QuadrantCircle RoundedBox Underline Label -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-