PartsListBuilderPartsListShowLockedDeletedRows Enumeration

NXOpen.Annotations.PartsListBuilder.PartsListShowLockedDeletedRows is an alias for NXOpen.Annotations.PartsListBuilderPartsListShowLockedDeletedRows

class NXOpen.Annotations.PartsListBuilderPartsListShowLockedDeletedRows

Bases: object

Locked deleted rows options The options specify how to show rows that are locked, but reference components that have been removed from the assembly

Enum Members

Enum Member Enum Member Description
Strikethrough
Blanked
Hidden
Ordinary
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.