OffsetCenterPointBuilderThickness Enumeration¶
NXOpen.Annotations.OffsetCenterPointBuilder.Thickness is an alias for NXOpen.Annotations.OffsetCenterPointBuilderThickness
-
class
NXOpen.Annotations.
OffsetCenterPointBuilderThickness
¶ Bases:
object
the valid types of offset center point thickness
Enum Members
Enum Member Enum Member Description Thin thin Normal normal Thick thick One Width One Two Width Two Three Width Three Four Width Four Five Width Five Six Width Six Seven Width Seven Eight Width Eight Nine Width Nine -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-