NarrowDisplayOption Enumeration¶
-
class
NXOpen.Annotations.
NarrowDisplayOption
¶ Bases:
object
Specifies the narrow dimension display option Enum Members
Enum Member Enum Member Description NotSet Doesn’t display narrow dimension NoLeader Displays narrow dimension without leader WithLeaderNoStub Displays narrow dimension with leader, but without stub AboveStub Displays narrow dimension above stub AfterStub Displays narrow dimension after stub Last Last enum value. Should not be used. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-