MasterCustomSymbolData Class¶
-
class
NXOpen.Annotations.
MasterCustomSymbolData
¶ Bases:
NXOpen.TransientObject
Represents master custom symbol data
New in version NX6.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.Annotations.MasterSymbolBuilder
instead.
Properties¶
Property | Description |
---|---|
Anchor | Returns or sets the anchor point |
PartName | Returns or sets the master part name |
SymbolName | Returns or sets the symbol name |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetPath | Get the path for part name |
SetGeometry | Specify the geometry for this master custom symbol data. |
SetPath | Set the valid path for part name |
Property Detail¶
Anchor¶
-
MasterCustomSymbolData.
Anchor
¶ Returns or sets the anchor point
-------------------------------------
Getter Method
Signature
Anchor
Returns: Anchor point Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Anchor
Parameters: anchor ( NXOpen.Point
) – New anchor pointNew in version NX6.0.0.
License requirements: None.
PartName¶
-
MasterCustomSymbolData.
PartName
¶ Returns or sets the master part name
-------------------------------------
Getter Method
Signature
PartName
Returns: The master part name Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PartName
Parameters: name (str) – New master part name New in version NX6.0.0.
License requirements: None.
SymbolName¶
-
MasterCustomSymbolData.
SymbolName
¶ Returns or sets the symbol name
-------------------------------------
Getter Method
Signature
SymbolName
Returns: Symbol name Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SymbolName
Parameters: name (str) – New symbol name New in version NX6.0.0.
License requirements: None.
Method Detail¶
Dispose¶
-
MasterCustomSymbolData.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX6.0.0.
License requirements: None.
GetPath¶
-
MasterCustomSymbolData.
GetPath
¶ Get the path for part name
Signature
GetPath()
Returns: Path Return type: str New in version NX7.5.2.
License requirements: None.
SetGeometry¶
-
MasterCustomSymbolData.
SetGeometry
¶ Specify the geometry for this master custom symbol data.
Signature
SetGeometry(geom)
Parameters: geom (list of NXOpen.DisplayableObject
) – symbol geometryNew in version NX6.0.0.
License requirements: None.