LineWeldDataBuilderWeldSymbolType Enumeration¶
NXOpen.Annotations.LineWeldDataBuilder.WeldSymbolType is an alias for NXOpen.Annotations.LineWeldDataBuilderWeldSymbolType
-
class
NXOpen.Annotations.
LineWeldDataBuilderWeldSymbolType
¶ Bases:
object
Represents the weld symbol type
Enum Members
Enum Member Enum Member Description NotSet ButtWeldWithRaisedEdges SingleFlange SquareButt VButt VButtWithBroadRootFace BevelButt BevelButtWithBroadRootFace UButt JButt FlareV FlareBevel KGroove Fillet Stake PlugSlot Edge Edge2 Spot Spot2 Seam Seam2 SteepFlankedVButt SteepFlankedBevelButt Backing SurfaceJoint SolderedJoint InclinedJoint FoldJoint Stud Surfacing Intermittent BackingPlate NotSpecified -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-