LeaderDataArrowheadType Enumeration¶
NXOpen.Annotations.LeaderData.ArrowheadType is an alias for NXOpen.Annotations.LeaderDataArrowheadType
-
class
NXOpen.Annotations.
LeaderDataArrowheadType
¶ Bases:
object
the set of arrowhead types used to define a leader arrowhead
Enum Members
Enum Member Enum Member Description ClosedArrow Closed arrowhead type ClosedSolidArrow Closed solid arrowhead type OpenArrow Open arrowhead type FilledArrow Filled arrowhead type ClosedDoubleArrow Closed double arrowhead type ClosedDoubleSolidArrow Closed double solid arrowhead type OpenDoubleArrow Open double arrowhead type FilledDoubleArrow Filled double arrowhead type NotSet No terminating symbol Origin Origin symbol Cross Cross symbol Integral Integral symbol Dot Dot symbol FilledDot Filled dot symbol Square Square symbol FilledSquare Filled square symbol Datum Datum symbol FilledDatum Filled datum symbol TopOpenArrow Top open arrowhead BottomOpenArrow bottom open arrowhead TopFilledArrow top filled arrowhead BottomFilledArrow bottom filled arrowhead -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-