ImportAutocadBlockBuilderType Enumeration¶
NXOpen.Annotations.ImportAutocadBlockBuilder.Type is an alias for NXOpen.Annotations.ImportAutocadBlockBuilderType
-
class
NXOpen.Annotations.
ImportAutocadBlockBuilderType
¶ Bases:
object
Symbol Type Enum. This option is used to differentiate OS, Teamcenter and Part symbols
Enum Members
Enum Member Enum Member Description Teamcenter Teamcenter Symbol Part Part Symbol Native OS Symbol -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-