IdentificationLineLocation Enumeration¶
-
class
NXOpen.Annotations.
IdentificationLineLocation
¶ Bases:
object
Specifies the weld identification line location (ISO and DIN only) Enum Members
Enum Member Enum Member Description NotSet Specifies no identification line Top Specifies identification line above the reference line Bottom Specifies identification line below the reference line Last Last enum value. Should not be used. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-