IdSymbolBuilderSymbolTypes Enumeration¶
NXOpen.Annotations.IdSymbolBuilder.SymbolTypes is an alias for NXOpen.Annotations.IdSymbolBuilderSymbolTypes
-
class
NXOpen.Annotations.
IdSymbolBuilderSymbolTypes
¶ Bases:
object
the valid types for an id symbol
Enum Members
Enum Member Enum Member Description Circle Circle DividedCircle Divided circle Triangle Triangle with point down TriangleUp Triangle with point up Square Square DividedSquare Divided square Hexagon Hexagon DividedHexagon Divided hexagon QuadrantCircle Quadrant circle RoundedBox Rounded box Underline Underline -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-