HoleTableSettingsWorkflowBuilder Class

class NXOpen.Annotations.HoleTableSettingsWorkflowBuilder

Bases: NXOpen.Annotations.TabularNoteStyleBuilder

Represents a NXOpen.Annotations.HoleTableSettingsWorkflowBuilder

New in version NX9.0.0.

Properties

Property Description
AutomaticUpdate Returns or sets the automatic update
LockTableContents Returns or sets the lock table contents
LockTableFormat Returns or sets the lock table format
ShowLockedDeletedContent Returns or sets the locked deleted row method
Tag Returns the Tag for this object.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Method Detail

Validate

HoleTableSettingsWorkflowBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.