HoleTableSettingsContentBuilder Class¶
-
class
NXOpen.Annotations.
HoleTableSettingsContentBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Annotations.HoleTableSettingsContentBuilder
New in version NX9.0.0.
Methods¶
Method | Description |
---|---|
GetContentOrder | Returns content order |
SetContentOrder | Sets content order |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
HoleTableSettingsContentBuilderContent Enumeration | Represents Content options |
Method Detail¶
GetContentOrder¶
-
HoleTableSettingsContentBuilder.
GetContentOrder
¶ Returns content order
Signature
GetContentOrder()
Returns: Return type: list of NXOpen.Annotations.HoleTableSettingsContentBuilderContent
New in version NX9.0.0.
License requirements: None.
SetContentOrder¶
-
HoleTableSettingsContentBuilder.
SetContentOrder
¶ Sets content order
Signature
SetContentOrder(contentOrder)
Parameters: contentOrder (list of NXOpen.Annotations.HoleTableSettingsContentBuilderContent
) –New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
Validate¶
-
HoleTableSettingsContentBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.