HoleCalloutSettingsBuilderLeaderAttachment Enumeration

NXOpen.Annotations.HoleCalloutSettingsBuilder.LeaderAttachment is an alias for NXOpen.Annotations.HoleCalloutSettingsBuilderLeaderAttachment

class NXOpen.Annotations.HoleCalloutSettingsBuilderLeaderAttachment

Bases: object

This reprensent the option that indicates the position for the leader to attach to.

Enum Members

Enum Member Enum Member Description
Top
BelowBottomExtendedToMaximum
BelowTopExtendedToMaximum
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.