HoleCalloutSettingsBuilderFeaturetype Enumeration¶
NXOpen.Annotations.HoleCalloutSettingsBuilder.Featuretype is an alias for NXOpen.Annotations.HoleCalloutSettingsBuilderFeaturetype
-
class
NXOpen.Annotations.
HoleCalloutSettingsBuilderFeaturetype
¶ Bases:
object
This reprensent the option that indicates a type of hole features.
Enum Members
Enum Member Enum Member Description GeneralHole DrillSizeHole ScrewClearanceHole ThreadedHole SymbolicThread NotSet -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-