GeometricCharacteristic Enumeration¶
-
class
NXOpen.Annotations.
GeometricCharacteristic
¶ Bases:
object
Specifies the geometric characteristic for an FCF Enum Members
Enum Member Enum Member Description Straightness Specifies straightnesss characteristics Flatness Specifies flatness characteristics Circular Specifies cirular characteristics Cylindrical Specifies cylindrical characteristics LineProfile Specifies line profile characteristics SurfaceProfile Specifies surface profile characteristics Angular Specifies angular characteristics Perpendicular Specifies perpendicular characteristics Parallel Specifies parallel characteristics Position Specifies position characteristics Concentric Specifies concentric characteristics Symmetric Specifies symmetric characteristics CircularRunout Specifies cirular runout characteristics TotalRunout Specifies total runout characteristics Last Last enum value. Should not be used. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-