GdtDatumCollection Class¶
-
class
NXOpen.Annotations.
GdtDatumCollection
¶ Bases:
object
Represents a collection of
NXOpen.Annotations.Datum
objectsTo obtain an instance of this class, refer to
NXOpen.Annotations.AnnotationManager
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
CreateDatum | Creates a PMI datum |
CreateDraftingDatumFeatureSymbolBuilder | Creates a NXOpen.Annotations.DraftingDatumFeatureSymbolBuilder |
CreatePmiDatumFeatureSymbolBuilder | Creates a NXOpen.Annotations.PmiDatumFeatureSymbolBuilder |
NewDatumData | Creates new DatumData object |
Method Detail¶
CreateDatum¶
-
GdtDatumCollection.
CreateDatum
¶ Overloaded method CreateDatum
CreateDatum(datumData, pmiData, annotationPlane, origin, leader)
CreateDatum(datumData, origin, leader)
-------------------------------------
Creates a PMI datum
Signature
CreateDatum(datumData, pmiData, annotationPlane, origin, leader)
Parameters: - datumData (
NXOpen.Annotations.DatumData
) – Datum data - pmiData (
NXOpen.Annotations.PmiData
) – PMI data - annotationPlane (
NXOpen.Xform
) – Annotation plane on which the datum lies - origin (
NXOpen.Point3d
) – Origin for the datum - leader (
NXOpen.Annotations.LeaderBundle
) – Specifies the leaders for the FCF The following leader types are not valid for Datum: PlainNostub and AlignedNostub
Returns: New datum
Return type: New in version NX4.0.0.
License requirements: geometric_tol (“GDT”)
-------------------------------------
Creates a drafting datum
Signature
CreateDatum(datumData, origin, leader)
Parameters: - datumData (
NXOpen.Annotations.DatumData
) – Datum data - origin (
NXOpen.Point3d
) – Origin for the datum - leader (
NXOpen.Annotations.LeaderBundle
) – Specifies the leaders for the FCF The following leader types are not valid for Datum: PlainNostub and AlignedNostub
Returns: New datum
Return type: New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)
-------------------------------------
CreateDraftingDatumFeatureSymbolBuilder¶
-
GdtDatumCollection.
CreateDraftingDatumFeatureSymbolBuilder
¶ Creates a
NXOpen.Annotations.DraftingDatumFeatureSymbolBuilder
Signature
CreateDraftingDatumFeatureSymbolBuilder(datum)
Parameters: datum ( NXOpen.Annotations.DraftingDatum
) – Datum to editReturns: Return type: NXOpen.Annotations.DraftingDatumFeatureSymbolBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
CreatePmiDatumFeatureSymbolBuilder¶
-
GdtDatumCollection.
CreatePmiDatumFeatureSymbolBuilder
¶ Creates a
NXOpen.Annotations.PmiDatumFeatureSymbolBuilder
Signature
CreatePmiDatumFeatureSymbolBuilder(datum)
Parameters: datum ( NXOpen.Annotations.Datum
) – Datum to editReturns: Return type: NXOpen.Annotations.PmiDatumFeatureSymbolBuilder
New in version NX6.0.0.
License requirements: geometric_tol (“GDT”)
NewDatumData¶
-
GdtDatumCollection.
NewDatumData
¶ Creates new DatumData object
Signature
NewDatumData()
Returns: New DatumData Return type: NXOpen.Annotations.DatumData
New in version NX4.0.0.
License requirements: None.