FrameBarElements Enumeration

class NXOpen.Annotations.FrameBarElements

Bases: object

Specifies the frame bar elements Enum Members

Enum Member Enum Member Description
AftPerpendicular
ForwardPerpendicular
CenterlineY
Baseline
Waterline
TransversalInsertArea
BulkHeads
Decks
TransverseFrames
InterTransverseFrames
LongitudinalYFrames
LongitudinalZFrames
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.