ForeshorteningSymbolSettingsBuilderMethodType Enumeration

NXOpen.Annotations.ForeshorteningSymbolSettingsBuilder.MethodType is an alias for NXOpen.Annotations.ForeshorteningSymbolSettingsBuilderMethodType

class NXOpen.Annotations.ForeshorteningSymbolSettingsBuilderMethodType

Bases: object

Represents foreshortening symbol method type

Enum Members

Enum Member Enum Member Description
WidthAndAngle
WidthAndHeight
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.