FlipOption Enumeration¶
-
class
NXOpen.Annotations.
FlipOption
¶ Bases:
object
Specifies the custom symbol flip option. This option is only available when editing. This option is unavailable for symbols with leaders. Enum Members
Enum Member Enum Member Description Horizontal Flips a symbol horizontally about a vertical line taken through its anchor point Vertical Flips a symbol vertically about a horizontal line taken through its anchor point Last Last enum value. Should not be used. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-