FitDisplayStyle Enumeration¶
-
class
NXOpen.Annotations.
FitDisplayStyle
¶ Bases:
object
Specifies the limit and fit display style Enum Members
Enum Member Enum Member Description FitSymbols Display only the grade and deviation FitSymbolsAndLimits Display grade, deviation, and limit values FitSymbolsAndTolerances Display grade, deviation, and tolerance values TolerancesOnly Display the tolerance values only -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-