FitAssemblyDisplayStyle Enumeration¶
-
class
NXOpen.Annotations.
FitAssemblyDisplayStyle
¶ Bases:
object
Specifies the limit and fit assembly display style This enum type is obsolete.
Deprecated since version NX11.0.0: Use
NXOpen.Annotations.FitAssemblyNewDisplayStyle
instead.Enum Members
Enum Member Enum Member Description SingleLine Display single line TwoLinesCentered Display hole and shaft with dimension text centered TwoLinesAligned Display hole and shaft with dimension text aligned -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-