FitAnsiHoleType Enumeration¶
-
class
NXOpen.Annotations.
FitAnsiHoleType
¶ Bases:
object
Specifies the limit and fit ANSI hole Enum Members
Enum Member Enum Member Description Hole Use hole values for the ANSI limit and fit tolerance Shaft Use shaft values for the ANSI limit and fit tolerance Fit Use fit values for the ANSI limit and fit tolerance -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-