FeatureControlFrameIndicatorBuilder Class¶
-
class
NXOpen.Annotations.
FeatureControlFrameIndicatorBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a FcfIndicatorBuilder
To create a new instance of this class, use
NXOpen.Annotations.AnnotationManager.CreateFeatureControlFrameIndicatorBuilder()
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
Direction | Returns or sets the direction |
IndicatorType | Returns or sets the indicator type |
Label | Returns the label |
Symbol | Returns or sets the charactersitic |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
FeatureControlFrameIndicatorBuilderFcfIndicatorCharacteristic Enumeration | Specifies the characteristic of the FCF indicator |
FeatureControlFrameIndicatorBuilderFcfIndicatorDirection Enumeration | Specifies the direction of the FCF indicator |
FeatureControlFrameIndicatorBuilderFcfIndicatorType Enumeration | Specifies the type of FCF indicator |
Property Detail¶
Direction¶
-
FeatureControlFrameIndicatorBuilder.
Direction
¶ Returns or sets the direction
-------------------------------------
Getter Method
Signature
Direction
Returns: Return type: NXOpen.Annotations.FeatureControlFrameIndicatorBuilderFcfIndicatorDirection
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Direction
Parameters: direction ( NXOpen.Annotations.FeatureControlFrameIndicatorBuilderFcfIndicatorDirection
) –New in version NX12.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
IndicatorType¶
-
FeatureControlFrameIndicatorBuilder.
IndicatorType
¶ Returns or sets the indicator type
-------------------------------------
Getter Method
Signature
IndicatorType
Returns: Return type: NXOpen.Annotations.FeatureControlFrameIndicatorBuilderFcfIndicatorType
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IndicatorType
Parameters: indicatorType ( NXOpen.Annotations.FeatureControlFrameIndicatorBuilderFcfIndicatorType
) –New in version NX12.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
Label¶
-
FeatureControlFrameIndicatorBuilder.
Label
¶ Returns the label
-------------------------------------
Getter Method
Signature
Label
Returns: Return type: NXOpen.Annotations.DatumReferenceBuilder
New in version NX12.0.0.
License requirements: None.
Symbol¶
-
FeatureControlFrameIndicatorBuilder.
Symbol
¶ Returns or sets the charactersitic
-------------------------------------
Getter Method
Signature
Symbol
Returns: Return type: NXOpen.Annotations.FeatureControlFrameIndicatorBuilderFcfIndicatorCharacteristic
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Symbol
Parameters: symbol ( NXOpen.Annotations.FeatureControlFrameIndicatorBuilderFcfIndicatorCharacteristic
) –New in version NX12.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
Method Detail¶
Validate¶
-
FeatureControlFrameIndicatorBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.