FeatureControlFrameDataBuilderToleranceZoneShape Enumeration¶
NXOpen.Annotations.FeatureControlFrameDataBuilder.ToleranceZoneShape is an alias for NXOpen.Annotations.FeatureControlFrameDataBuilderToleranceZoneShape
-
class
NXOpen.Annotations.
FeatureControlFrameDataBuilderToleranceZoneShape
¶ Bases:
object
Specifies the zone shape for the feature control frame
Enum Members
Enum Member Enum Member Description NotSet no zone shape Diameter diameter SphericalDiameter spherical diameter Square square -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-