FeatureControlFrameDataBuilderToleranceMaterialModifier Enumeration¶
NXOpen.Annotations.FeatureControlFrameDataBuilder.ToleranceMaterialModifier is an alias for NXOpen.Annotations.FeatureControlFrameDataBuilderToleranceMaterialModifier
-
class
NXOpen.Annotations.
FeatureControlFrameDataBuilderToleranceMaterialModifier
¶ Bases:
object
Specifies the tolerance material modifier condition
Enum Members
Enum Member Enum Member Description NotSet no material modifier LeastMaterialCondition least material condition MaximumMaterialCondition maximum material condition RegardlessOfFeatureSize regardless of feature size condition -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-