FeatureControlFrameDataBuilderAreaSymbolType Enumeration

NXOpen.Annotations.FeatureControlFrameDataBuilder.AreaSymbolType is an alias for NXOpen.Annotations.FeatureControlFrameDataBuilderAreaSymbolType

class NXOpen.Annotations.FeatureControlFrameDataBuilderAreaSymbolType

Bases: object

Specifies the unit type

Enum Members

Enum Member Enum Member Description
Rectangular Rectangular
Circular Circular
Spherical Spherical
Square Square
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.