EditTitleBlockBuilder Class¶
-
class
NXOpen.Annotations.
EditTitleBlockBuilder
¶ Bases:
NXOpen.Annotations.BaseTitleBlockBuilder
Represents a
NXOpen.Annotations.EditTitleBlockBuilder
builderTo create a new instance of this class, use
NXOpen.Annotations.TitleBlockCollection.CreateEditTitleBlockBuilder()
New in version NX8.0.0.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCellValueForLabel | Return the value of the cell for given label. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetCellValueForLabel | Sets the value of the cell for given label. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
GetCellValueForLabel¶
-
EditTitleBlockBuilder.
GetCellValueForLabel
¶ Return the value of the cell for given label.
If multiple title blocks are selected, then value of the cell from the first title block, which has the cell with given label, is returned.
Signature
GetCellValueForLabel(label)
Parameters: label (str) – Label whose value is queried Returns: Value of the label Return type: str New in version NX8.0.0.
License requirements: None.
SetCellValueForLabel¶
-
EditTitleBlockBuilder.
SetCellValueForLabel
¶ Sets the value of the cell for given label.
If multiple title blocks are selected, then values of cells with the given label in all the title blocks are set.
Signature
SetCellValueForLabel(label, value)
Parameters: - label (str) – Label whose value is to be set
- value (str) – Value of the label
New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
Validate¶
-
EditTitleBlockBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.