EditSymbolDisplayBuilderWidthTypes Enumeration¶
NXOpen.Annotations.EditSymbolDisplayBuilder.WidthTypes is an alias for NXOpen.Annotations.EditSymbolDisplayBuilderWidthTypes
-
class
NXOpen.Annotations.
EditSymbolDisplayBuilderWidthTypes
¶ Bases:
object
The Enum represent width types
NXOpen.Annotations.EditSymbolDisplayBuilder.Width()
andNXOpen.Annotations.EditSymbolDisplayBuilder.Width()
will set this width type at builder side and will be used to apply the same on the selected contents after commitEnum Members
Enum Member Enum Member Description Thin Thin Normal Normal Thick Thick ThicknessOne Width One ThicknessTwo Width Two ThicknessThree Width Three ThicknessFour Width Four ThicknessFive Width Five ThicknessSix Width Six ThicknessSeven Width Seven ThicknessEight Width Eight ThicknessNine Width Nine -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-