DraftingSurfaceFinishCollection Class¶
-
class
NXOpen.Annotations.
DraftingSurfaceFinishCollection
¶ Bases:
object
Represents a collection of
NXOpen.Annotations.DraftingSurfaceFinish
objectsTo obtain an instance of this class, refer to
NXOpen.Annotations.AnnotationManager
New in version NX7.5.0.
Methods¶
Method | Description |
---|---|
CreateDraftingSurfaceFinishBuilder | If None create a new Drafting Surface Finish, otherwise edit existing Drafting Surface Annotatation |
FindObject | Finds the drafting surface finish with the given name. |
Method Detail¶
CreateDraftingSurfaceFinishBuilder¶
-
DraftingSurfaceFinishCollection.
CreateDraftingSurfaceFinishBuilder
¶ If None create a new Drafting Surface Finish, otherwise edit existing Drafting Surface Annotatation
Signature
CreateDraftingSurfaceFinishBuilder(draftingSurfaceFinish)
Parameters: draftingSurfaceFinish ( NXOpen.Annotations.DraftingSurfaceFinish
) – surface finishReturns: Return type: NXOpen.Annotations.DraftingSurfaceFinishBuilder
New in version NX7.5.0.
License requirements: None.
FindObject¶
-
DraftingSurfaceFinishCollection.
FindObject
¶ Finds the drafting surface finish with the given name.
An exception will be thrown if no object can be found with given name
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier of the drafting surface finish to be found Returns: drafting surface finish with this identifier Return type: NXOpen.Annotations.DraftingSurfaceFinish
New in version NX7.5.0.
License requirements: None.