DraftingNoteBuilderTextAlign Enumeration¶
NXOpen.Annotations.DraftingNoteBuilder.TextAlign is an alias for NXOpen.Annotations.DraftingNoteBuilderTextAlign
-
class
NXOpen.Annotations.
DraftingNoteBuilderTextAlign
¶ Bases:
object
text over leader types for text
Enum Members
Enum Member Enum Member Description Top Align top Middle Align middle Bottom Align bottom BelowbottomExtToMax Align below bottom extension to maximum BelowbottomExtToMaxUnderline Align below bottom extension to maximum and underline Belowbottom Align below bottom BelowbottomUnderline Align below bottom and underline BelowTopExtToMax Align below top extension to maximum BelowTopExtToMaxUnderline Align below top extension to maximum and underline BelowTop Align below top BelowTopUnderline Align below top and underline -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-