DisplayStyleBuilder Class¶
-
class
NXOpen.Annotations.
DisplayStyleBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Annotations.DisplayStyleBuilder
.This is a sub-builder class and cannot be directly instantiated
New in version NX11.0.1.
Properties¶
Property | Description |
---|---|
LockSizeAndPosition | Returns or sets the PMI lock pan and zoom setting |
ParallelToScreen | Returns or sets the PMI parallel to screen setting |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
LockSizeAndPosition¶
-
DisplayStyleBuilder.
LockSizeAndPosition
¶ Returns or sets the PMI lock pan and zoom setting
-------------------------------------
Getter Method
Signature
LockSizeAndPosition
Returns: Return type: bool New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
LockSizeAndPosition
Parameters: lockSizeAndPosition (bool) – New in version NX11.0.1.
License requirements: geometric_tol (“GDT”)
ParallelToScreen¶
-
DisplayStyleBuilder.
ParallelToScreen
¶ Returns or sets the PMI parallel to screen setting
-------------------------------------
Getter Method
Signature
ParallelToScreen
Returns: Return type: bool New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ParallelToScreen
Parameters: parallelToScreen (bool) – New in version NX11.0.1.
License requirements: geometric_tol (“GDT”)
Method Detail¶
Validate¶
-
DisplayStyleBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.