DimensionUnit Enumeration¶
-
class
NXOpen.Annotations.
DimensionUnit
¶ Bases:
object
Specifies the dimension unit Enum Members
Enum Member Enum Member Description Millimeters Specifies millimeters units Meters Specified meters units Inches Specifies inches units ArchitecturalFeetInches Specified architectural units - converts inches to feet for measurements larger than 12 inches EngineeringFeetInches Specified engineering units - converts inches to feet for measurements larger than 72 inches Last Last enum value. Should not be used. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-