DimensionType Enumeration¶
-
class
NXOpen.Annotations.
DimensionType
¶ Bases:
object
Specifies the type of dimension being created Enum Members
Enum Member Enum Member Description AngularMajor Major Angular dimension AngularMinor Minor Angular dimension ArcLength Arc Length dimension Baseline Baseline dimension Chain Chain dimension Chamfer Chamfer dimension ConcentricCircle Concentric Circle dimension Cylindrical Cylindrical dimension Diameter Diameter dimension FoldedRadius Folded Radius dimension Hole Hole dimension Horizontal Horizontal dimension OrdinateHorizontal Horizontal Ordinate dimension OrdinateOrigin Ordinate Origin dimension OrdinateVertical Vertical Ordinate dimension Parallel Parallel dimension Perpendicular Perpendicular dimension Radius Radius dimension Vertical Vertical dimension Last Last enum value. Should not be used. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-