DimensionMeasurementBuilderMeasurementMethod Enumeration¶
NXOpen.Annotations.DimensionMeasurementBuilder.MeasurementMethod is an alias for NXOpen.Annotations.DimensionMeasurementBuilderMeasurementMethod
-
class
NXOpen.Annotations.
DimensionMeasurementBuilderMeasurementMethod
¶ Bases:
object
measurement method for the dimensions
Enum Members
Enum Member Enum Member Description Inferred Inferred measurement direction (UI Only) Horizontal Horizontal measurement direction Vertical Vertical measurement direction PointToPoint Point to point measurement direction Perpendicular Perpendicular measurement direction Cylindrical Linear measurement method representing a diameter Angular Angular measurement type Radial Radial measurement type Diametral Diametral measurement type HoleCallout Hole Callout based measurement -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-