DatumTargetBuilderTerminatorTypes Enumeration¶
NXOpen.Annotations.DatumTargetBuilder.TerminatorTypes is an alias for NXOpen.Annotations.DatumTargetBuilderTerminatorTypes
-
class
NXOpen.Annotations.
DatumTargetBuilderTerminatorTypes
¶ Bases:
object
represents the datum target terminator type
Enum Members
Enum Member Enum Member Description Arrow terminated with Arrow only X terminated with x Plus terminated with plus -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-