DatumTargetBuilderStandardTypes Enumeration¶
NXOpen.Annotations.DatumTargetBuilder.StandardTypes is an alias for NXOpen.Annotations.DatumTargetBuilderStandardTypes
-
class
NXOpen.Annotations.
DatumTargetBuilderStandardTypes
¶ Bases:
object
represents the datum target standards
Enum Members
Enum Member Enum Member Description NoStandard NO_STANDARD AsmeY145m1982 ASME_Y145M_1982 AsmeY145m1994 Y145M_1994 AsmeIso11011983 ISO 1101 1983 GmAddendum94 94_GM_ADDENDUM Asig2000 ASIG_2000 AsmeY1452009 ASME_Y145_2009 -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-